Schaeffler Expands Line of Aftermarket Bearings, Seals and Housing Units for Agricultural Equipment

2022-05-02 | Valley City, Ohio
- Schaeffler is now offering both metric and imperial bearings to the agricultural aftermarket
- Less downtime and longer work cycles for agricultural equipment
- OE-quality heavy-duty bearings provide improved anti-corrosion protection for significantly increased operating life
Leading automotive and industrial supplier Schaeffler is launching a range of aftermarket bearings, seals and housings for the agricultural equipment and machinery market.
Schaeffler’s comprehensive line of OE-quality bearings are specifically engineered to the precise performance parameters of agricultural applications, including tractors, harvesters, and tillage machines. Reliable and dependable bearing solutions are critical in minimizing equipment downtime. Schaeffler’s heavy-duty bearings are designed to support the constant vibrations and high shock loads of agricultural machinery.
The bearings feature a unique corrosion protection system – Schaeffler’s Corrotect® coating – which facilitates reliable operation in every environment and helps increase the operating life of heavy equipment and machinery. The three-piece seal concept retains the high-quality grease and helps prevent contamination and moisture from reaching the interior of the bearing.
Schaeffler is further expanding its product line with metric-sized bearings and is now providing both metric and imperial-sized bearings for agricultural applications in North America. Equipment owners and operators can now choose from over 200 easy-to-mount options for a diameter range of 10 to 120 mm. The new metric offering compliments Schaeffler’s existing line of imperial-sized bearings, which already includes over 400 SKUs.
Product Portfolio
Aftermarket bearings for agricultural applications include radial insert ball bearings and housing units, sealed deep groove ball bearings and angular contact ball bearings, tapered roller bearings, and bearings with hexagonal and square bores.
For more information on the product line and technical specifications, please download the Radial Insert Ball Bearing and Housing Units product catalog.
Publisher: Schaeffler Group USA Inc.
Country: USA
Usage of Schaeffler press pictures
Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.
We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.
Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.
Postal adress:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestraße 1-3
91074 Herzogenaurach
Germany
Press releases
Package (Press release + media)