Search term

Schaeffler expands its OPTIME Ecosystem portfolio: Smart FAG OPTIME C4 lubricator now available

With FAG OPTIME C4, several lubrication points can be supplied at the same time and more lubricant can be stored. This opens up a wider range of applications for maintenance teams in the maintenance of their machinery. Image:Schaeffler
With FAG OPTIME C4, several lubrication points can be supplied at the same time and more lubricant can be stored. This opens up a wider range of applications for maintenance teams in the maintenance of their machinery. Image: Schaeffler

2025-09-30 | Fort Mill, S.C.

  • New addition to the portfolio: Smart FAG OPTIME C4 lubricator with four independent outlets for reliable lubricant supply
  • Increased outlet pressure and larger fill volume provide greater flexibility in maintenance
  • When used in combination with the OPTIME app, incorrect lubrication can be reliably prevented

Rolling bearings depend on optimal lubrication to ensure long-term, reliable operation. In practice, however, manual relubrication is still part of the daily routine for many maintenance teams, and errors in this process remain one of the leading causes of bearing failures.

This is precisely where Schaeffler, the Motion Technology Company, provides solutions with its lubricators. The latest development in the portfolio, the FAG OPTIME C4, is capable of simultaneously supplying several lubrication points while storing a greater quantity of lubricant. For maintenance teams, this opens up broader application possibilities in servicing their machinery fleet.

FAG OPTIME C4 supplies up to four lubrication points
As a multi-point lubricator, the FAG OPTIME C4 features four outlets that can be programmed independently of one another. This allows a single lubricator to supply up to four lubrication points individually. As a result, only one device needs to be purchased, configured, and maintained to cover several points. In addition, both the outlet pressure and the fill volume of the lubricant cartridges are significantly higher.

The FAG OPTIME C4 delivers an outlet pressure of 70 bar (1,015 psi), allowing lubricant to be transported over longer distances and reaching lubrication points that cannot be fitted with a lubricator nearby. Even machines that, by design, generate higher back pressure can now be lubricated intelligently.

The FAG OPTIME C4 can hold 400 or 750 cm³ of grease, or 850 cm³ of oil. Thanks to the larger fill volume, cartridges require replacement or refilling far less often. As a result, even lubrication points with high lubricant requirements can now be supplied by a single intelligent lubricator. This option was rarely economical in the past due to the effort involved in frequent refilling. As a result, the FAG OPTIME C4 is particularly well suited for demanding applications such as mining, where it can also be used as a single-point lubrication system, or for oil lubrication of drive chains.

In combination with Schaeffler’s OPTIME app (available in the Apple App Store and on Google Play), the FAG OPTIME C4 ensures that incorrect lubrication can be safely avoided, whether caused by too much or too little lubricant, the wrong lubricant, contamination, clogged lubricant lines, or empty cartridges.

The OPTIME Ecosystem: Solutions for condition monitoring and lubrication
Schaeffler’s OPTIME Ecosystem comprises a range of solutions for condition monitoring and smart lubrication. In late 2021, the portfolio was expanded with the introduction of the OPTIME C1 lubricator, enabling smart lubrication management for the first time. The new FAG OPTIME C4 now adds an even more flexible and powerful option to the lineup. Solutions within the OPTIME Ecosystem are cost-efficient, wireless, app-controlled, scalable, and suitable for a wide variety of drive systems.

The FAG OPTIME C4 will be available to order starting September 25, 2025, in most countries across Europe, North and South America, and the Asia-Pacific region.

Further information about this product is available here: Smart Lubrication Systems OPTIME C1 and FAG OPTIME C4 | Schaeffler medias.

Publisher: Schaeffler Group US
Country: USA

Related media

Usage of Schaeffler press pictures

Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.

We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.

Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.

Postal adress:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestraße 1-3
91074 Herzogenaurach
Germany

presse@schaeffler.com

Downloads

Package (Press release + media)

Share Page

Schaeffler applies cookies to secure an optimal use. With the further use of this website you accept the application of cookies. More Information

Accept