Search term

CES 2026 Schaeffler presents innovative planetary gear actuator for humanoid robots

Schaeffler’s planetary gear actuator is a highly efficient drive system that enables precise and energy-efficient motion sequences. Image: Schaeffler
Schaeffler’s planetary gear actuator is a highly efficient drive system that enables precise and energy-efficient motion sequences. - Image: Schaeffler

2025-12-16 | Las Vegas/ Herzogenaurach

  • Schaeffler’s planetary gear actuator ensures precise movements in robot joints and enables continuous-duty operation
  • Innovative actuator system combines a two-stage planetary gearbox, electric motor, encoder, and controller in a compact unit
  • Decades of Schaeffler actuator expertise make humanoid robots even more capable and powerful

World premiere at the Consumer Electronics Show 2026 (CES) in Las Vegas: For the first time, Schaeffler is presenting a planetary gear actuator developed specifically for humanoid robots at a leading global trade fair. Actuators transmit torque with high precision and minimal compliance and are essential for enabling humanoid robots to move accurately and efficiently. On average, 25 to 30 actuators are required in total for joints such as the shoulders, knees, and hips. While conventional actuators often offer limited or no back-drive-ability – that is, the ability to move the drive in reverse – Schaeffler’s planetary gear actuator enables smooth back-driving and high precision thanks to its innovative design. In addition, Schaeffler manufactures all components entirely in-house, ensuring the highest levels of quality and reliability. Humanoid robots will play a key role in the industry of tomorrow, as they can be seamlessly integrated into existing work environments, relieve employees of repetitive and ergonomically demanding tasks, and significantly increase productivity as a result.

Andreas Schick, Chief Operating Officer of Schaeffler AG and responsible on the Executive Board for humanoid activities, says: “Schaeffler aims to secure a key position in the rapidly growing humanoid robotics market. Thanks to our decades of manufacturing expertise, we are able to deliver the highest quality in large volumes and within the shortest possible production times. The innovative planetary gear actuator is a production-ready key product within our portfolio and will make humanoid robots even more capable and powerful.”

Planetary gear actuator: A tailor-made drive solution for humanoid robots
Schaeffler deploys humanoid robots across its entire value chain and therefore understands market requirements and customer needs firsthand. This enables Schaeffler to successfully transfer scalable solutions from the automotive and industrial sectors to humanoid robotics and to develop tailor-made products that address the challenges of the future. With a comprehensive portfolio spanning eight product families, Schaeffler covers the full spectrum of requirements for humanoid robots. Integrated linear and rotary actuators – one of Schaeffler’s core competencies – account for around half of all components in a humanoid robot. This highlights the company’s strong vertical integration and its concentrated expertise as a Motion Technology Company.

One of the product highlights of this year’s CES trade show is the planetary gear actuator, a highly efficient drive system designed and manufactured entirely by Schaeffler. The compact yet powerful system combines a two-stage planetary gearbox, an electric motor, as well as an encoder and controller in a space-optimized unit. Thanks to its high thermal stability, a torque range of 60 to 250 Nm, and particularly low back-drive-ability, the planetary gear actuator withstands external forces and prevents unintended reverse rotation of the drive component. The result is precise, energy-efficient motion sequences with high torque transparency – ideal for continuous-duty operation in humanoid robots.

Schaeffler at the Consumer Electronics Show
Innovative key components for humanoid robots, along with other future technologies from Schaeffler, will be on display from January 6 to 9, 2026, in the West Hall of the Las Vegas Convention Center at Booth 7301.

Learn more about Schaeffler’s appearance at the Consumer Electronics Show:
CES 2026 | Dates & Events | Schaeffler Group USA Inc.

Publisher: Schaeffler Group USA Inc.
Country: USA

Related media

Usage of Schaeffler press pictures

Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.

We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.

Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.

Postal adress:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestraße 1-3
91074 Herzogenaurach
Germany

presse@schaeffler.com

Downloads

Package (Press release + media)

Share Page

Schaeffler applies cookies to secure an optimal use. With the further use of this website you accept the application of cookies. More Information

Accept