Schaeffler Introduces CONCEPT1 Single-Point Automatic Lubricator

2020-10-15 | Fort Mill, South Carolina
- CONCEPT1 single-point automatic lubricator now available in North America
- Engineered to ensure optimal lubrication and improve reliability of electric motors and other industrial machines
- Accommodates a variety of lubricant options, including Schaeffler’s comprehensive lineup of proprietary ArcanolTM lubricating greases
Global industrial and automotive supplier Schaeffler is launching its innovative CONCEPT1 single-point automatic lubricator to the North American market.
Engineered to ensure optimal lubrication in a broad range of industrial machines and devices – including electric motors, bearing housings, fans, blowers and pumps – CONCEPT1 from Schaeffler eliminates the need for time-consuming manual lubrication procedures, while preventing lubrication mistakes such as over- or under-greasing that can cause unplanned plant equipment downtime.
“Approximately 60% of electric motor failures can be traced to bearing-related problems that are typically due to lubrication issues,” says David French, product manager for Industry 4.0 solutions at Schaeffler. “Accordingly, we designed CONCEPT1 to provide our customers with a versatile and easy-to-use solution that delivers the right grease in the right quantity at just the right intervals.”
Schaeffler’s CONCEPT1 single-point lubricator uses an electrochemical reaction to precisely and continuously supply the proper amount of lubricant to rolling bearings inside electric motors and other industrial machinery. Easy to install and operate, CONCEPT1 can reduce plant maintenance costs by as much as 25% when compared to manual lubrication procedures.
CONCEPT1 is available pre-filled with Schaeffler’s industry-leading line of Arcanol greases, or customers can have CONCEPT1 filled at the factory with an extensive selection of name-brand and special-order lubricants. Alternatively, customers can purchase empty lubricant cartridges for CONCEPT1 and use their own grease. To reduce waste and help protect the environment, CONCEPT1 can be refilled up to three times using Schaeffler’s specially designed refill kits.
Publisher: Schaeffler Group USA Inc.
Country: USA
Usage of Schaeffler press pictures
Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.
We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.
Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.
Postal adress:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestraße 1-3
91074 Herzogenaurach
Germany
Press releases
Package (Press release + media)