Schaeffler Group USA Inc. · USA

 
 

Welcome To Schaeffler Group North America

Schaeffler Group North America is responsible for the engineering, production, sales and marketing for the INA, LuK, FAG and Barden brands throughout the United States, Canada, Mexico, Central America and the Caribbean. Manufacturing a full line of rolling bearings, engine and drivetrain components, linear motion products, precision products and plain bearings, we service the Automotive OEM, Industrial OEM and Distribution markets, as well as the Aerospace industry. Our extensive product portfolio is further supplemented by a full range of condition monitoring and maintenance products to support your overall bearing maintenance requirements.

 

Current messages

2010-07-16 | LIBRARY

Driven Linear Units

Transport and positioning in sophisticated feed and discharge processes places particular requirements on the components and system construction. We have developed compact, highly integrated linear actuators and linear tables to fulfil these requirements.

Product range
 
2010-06-09 | PRESS

Slippage? – No problem!

Slippage is the natural enemy of bearings. Schaeffler Group Industrial is presenting its first rolling bearing that is not only resistant to the effects of slippage but also prevents slippage from occurring in the first place – the new FAG tube roller bearing. The special feature of this bearing is that it contains three newly developed tube rollers instead of conventional rolling elements.

FAG tube roller bearings
 
2010-05-27 | PRESS

Multi-Body Simulation Makes Wind Energy More Efficient

Rolling bearing supports in wind turbines are subjected to high, extremely alternating loads and a wide range of low and high speeds depending on the installation point. They are at the core of the drive train and therefore of the entire turbine. Accordingly, rolling bearing development takes account of the entire wind turbine system with the dependencies and interactions of its individual drive train components.

Virtual prototyping for wind turbine design
 
2010-05-27 | PRESS

Bearings for wind tracking and blade adjustment

Wind turbines must be aligned to the wind conditions. The tower and the rotor blades are adjusted so that they make optimal use of the wind conditions and are not subject to excessive loads that could cause damage. Tower and blade adjustment are therefore significant prerequisites for cost-effective operation of wind turbines.

Slewing rings for exact positioning
 
2010-05-11 | PRESS

The Schaeffler Group is among the top five leaders in innovation

With 1,146 registered patents, the Schaeffler Group ranks fifth in the German Patent and Trademark Office’s list of patent applicants that is published annually. In this list, 747 patents are for new products from Schaeffler Technologies GmbH & Co. KG with its brands INA and FAG and 399 patents are from the Schaeffler brand LuK.

New patents for numerous innovations for passenger cars and industrial sectors
 
2010-04-30 | PRESS

“Schaeffler Hybrid” – a car full of ideas for e-mobility

The Schaeffler Group has developed a car full of ideas called the “Schaeffler Hybrid”. The vehicle is part of an advance development project that enables a practical comparison of the various options available for e-mobility to be made. The vehicle demonstrates various vehicle configurations and driving conditions. This means the Schaeffler Hybrid not only has a volume produced combustion engine from a basic vehicle, but also has a central electric motor and two wheel hub motors.

Schaeffler presents product portfolio for electric mobility as part of a variable advance development project
 
2010-04-28 | LIBRARY

Axial/Radial Bearings

The double direction axial bearings suitable for flange mounting and with a radial guidance component correspond essentially in their design, mounting dimensions, rigidity and load carrying capacity to the established YRT bearings. As in the case of the latter bearings, they can support high radial forces, axial loads from both directions and tilting moments free from clearance and with high rigidity.

For applications with reduced accuracy requirements
 
SERVICE
 

Catalog | 2008-12
Product Reference Guide (PRG)

 
medias® 5.0
PRODUCT CATALOG

Quickly and easily with our selection assistants:
medias® product selection and information system has been completely revised.

medias 5.0 Product Catalog

 
SERVICE
 

Catalog | 2009-11
Large Size Bearings (GL1)
Ball bearings Roller bearings Back-up rollers Spherical plain bearings Bearing housings Accessories