Search term

Simulation, Calculation and Test

Optimum Design

State-of-the-art Calculation and Simulation Programs

Our specialists work in close cooperation with wind turbine developers, manufacturers, and operators. State-of-the-art calculation and simulation programs ensure that optimum designs for bearings for wind power applications are produced. The entire system is considered, from individual rolling bearings and their components and adjacent construction through to the entire power transmission system, which is displayed and optimized using multi-body simulation programs developed in-house.

With its realistic force and torque simulation, Astraios has been providing valuable results since 2011, which are used for the new development of bearing solutions and for the optimization of the simulation and calculation models.

Optimum design with state-of-the-art calculation and simulation programs
Optimum design with state-of-the-art calculation and simulation programs
Schaeffler Calculation Chain

From Complete Systems to the Rolling Contact

Schaeffler calculation chain: from complete systems to the rolling contact

The Schaeffler calculation chain includes CAE tools that are perfectly suited to the specific requirements of the design.

  • SIMPLA: system simulation with rolling bearing expertise
  • BEARINX: bearing design with an understanding of systems
  • CABA3D: a dynamic view inside the bearing
  • TELOS: where the focus is on contact

SIMPLA: system simulation

SIMPLA – system simulation with rolling bearing expertise
SIMPLA – system simulation with rolling bearing expertise

With the hybrid multi-body simulation (MBS), the dynamic behavior of the entire wind turbine is displayed.

Based on the model, individual components of the drive train and the entire turbine design can be improved as early as the development phase.

  • Hybrid multibody simulation (MBS) with a non-linear, multi-dimensional coupled bearing model
  • MBS model can be derived from existing BEARINX model

BEARINX: optimum bearing design

BEARINX – bearing design with an understanding of systems
BEARINX – bearing design with an understanding of systems

With the BEARINX software, all bearing types, complex shafts, and shaft systems through to complete drive units can be modeled and calculated.

Amongst others, BEARINX considers the following factors:

  • Non-linear elastic deflection behavior of the bearings
  • The deflection of shafts and axes
  • The deflection of housings and adjacent components
  • The operating clearance or the preload of the bearings
  • Roller and raceway profiling as well as raceway osculation
  • Actual contact pressure considering tilted and profiled rolling elements
  • The influence of lubricant conditions, contamination and actual contact pressure on the fatigue life.

CABA3D: rolling bearing simulation

  • Dynamic analysis of rolling bearings
  • Determination of force and motion patterns of the rolling elements and rings, taking all degrees of freedom into consideration
  • CABA3D facilitates the calculation of the frictional energy and the acceleration behavior of the rolling elements, e.g. when they enter the load zone.

TELOS: rolling contact simulation

TELOS – where the focus is on contact
TELOS – where the focus is on contact
  • 3D rolling contact simulation program
  • Any contact under general lubrication conditions
  • Quasi-stationary as well as transient load conditions
  • Coated and uncoated bearing components

FEM

FEM calculations
FEM calculations

For even more detailed analyses, FEM calculations can determine the influence of the adjacent construction on the bearings and vice-versa.

Large-size Bearing Test Rig Astraios

Increased Reliability and Cost-effectiveness for Wind Turbines

Large-size bearing test rig ASTRAIOS
Large-size bearing test rig ASTRAIOS

One of the world’s largest, most up-to-date, and most powerful large-size bearing test rigs enables bearings of up to 15 tons and measuring up to 3.5 meters to be tested in realistic conditions using a comprehensive simulation program. ASTRAIOS will result in further improvements in the understanding of systems as a whole, influencing factors and the interrelations in the drive trains of wind turbines. This means Schaeffler is making a major contribution to shortening development times for wind turbines as well as making the design process more reliable and increasing the cost-effectiveness and safety of these turbines.

The test rig has been named “Astraios” after a Titan in Greek mythology who was father of the four wind gods.

Realistic force and moment simulation

Wind turbines are constantly subjected to changing wind conditions - from calm weather to storms ASTRAIOS simulates the real loads and moments which occur in a wind turbine.

  • For rotor bearings and slewing rings
  • All rotor bearing support concepts can be tested
  • For wind turbines of up to 6 MW

Comprehensive analysis

Over 300 sensors in the test bearings provide information to be evaluated for a variety of analyses. The measurement and control technology are provided by SARA, the automation system for R&D applications from Schaeffler. Our experts evaluate the data and improve the calculation models through comparison with the test results.

Share Page

Schaeffler applies cookies to secure an optimal use. With the further use of this website you accept the application of cookies. More Information

Accept