Search term

Customer Success Story

Sawing without unwanted interruptions – SmartChecks ensure wood processing in Sweden

Customer benefits

  • No costs incurred by production stoppages
  • Low system acquisition costs
  • Reduced maintenance costs
  • Increased plant availability
  • Greater security due to self-reporting system
Sector:
Wood processing industry
Application:
Motors
Product solution:
Condition Monitoring solution
Mikael Eriksson, operator of the Kåge sawmill
Mikael Eriksson, operator of the Kåge sawmill, is delighted.

Thanks to the SmartCheck, unexpected motor failures are almost entirely prevented. We can now see immediately if something is not right, such as unusual temperature increases or significantly changed vibrations for example, and can intervene before major problems arise. As a result, downtime costs of approx. EUR 20,000, as incurred in the most recent incident, are a thing of the past.

Challenge

Challenge

Running motors in the Norra Timber sawmill are a fundamental requirement for the smooth production of sawn timber. During this process, the bearings in the motors are subject to particular stress. When the main motor failed, the plant was brought to a standstill, and it took several hours before operations could resume. A failure of this kind can impact on the entire supply chain. In order to avoid such incidents in future, the sawmill operator sought a proactive solution.

Solution

Solution

Schaeffler experts on site recommended the use of the SmartCheck for motor monitoring. The SmartCheck is an online measuring system for monitoring machinery and process parameters. This maintenance solution enables early alarm triggering and visualization of potential damage, thus allowing maintenance work to be planned on a specific and proactive basis.

Special features of the project

Special features of the project

Schaeffler has been supplying roller bearings to the Norra Timber plant through local Schaeffler sales partner Sesemic for years. By using the Schaeffler condition monitoring solution, the sawmill operator is once again placing its trust in Schaeffler’s expertise. This maintenance solution can also be applied and expanded to other units such as fans, pumps, gearboxes, compressors, and machine tools in practically every plant across all sectors.

Customer

Customer

The Norra Timber sawmill in Kåge is one of the largest wood processing companies in Northern Sweden. Approximately 240,000 m³ of wood are processed into sawn timber every year and shipped to customers all over the world.

Sawmill control center
Sawmill control center
Commissioning of the SmartCheck on the main motor
Commissioning of the SmartCheck on the main motor
Schaeffler SmartCheck in action
Schaeffler SmartCheck in action

Our solution products

SmartCheck from Schaeffler

The SmartCheck from Schaeffler is a compact, innovative, modular online measuring system for continuous monitoring of machinery and process parameters on a decentralized basis.

Product page Schaeffler SmartCheck

Further information

Details to the success story


This may be of interest to you

Costs saved

Automatic lubricators and the change to quality grease Arcanol MULTITOP prevent failures of the wide belt grinding machine.

The drinking water supplier Perlenbach relies on Schaeffler solutions for the maintenance of its pumps.

We are here for you!

Do you have questions about Schaeffler, our products and services, or wish to receive further information?

Your personal sales representative will assist you with any inquiries.

Please contact us

Share Page

Schaeffler applies cookies to secure an optimal use. With the further use of this website you accept the application of cookies. More Information

Accept