Schaeffler North America

 
 
 
 
 
 
PUBLICATIONS
 

Brochure | 2011-08
Infrared thermography as a service
Taking the heat out of maintenance

 
 

Catalog | 2015-07
Mounting and Maintenance of Rolling Bearings
Products Services Training

 
CONTACT
 
Measurement Methods

Thermography

Thermography is one of the most important non-destructive diagnostic techniques, Figure 5 . Many technical problems manifest themselves in the form of heat generation, which can be detected with the aid of a high resolution infrared camera. The major advantage of thermography is the rapid, non-contact collection of temperature data.

 

If a photograph is taken at the same time, the temperature patterns present in a machine part can be assigned on site.

 

Thermography can be used for assessment in relation to numerous objects, such as in the case of:

  • non-contact monitoring of rolling bearings during operation
  • thermal monitoring of processes
 

Schaeffler applies cookies to secure an optimal use. With the further use of this website you accept the application of cookies. More Information

Accept