Schaeffler Group USA Inc. · USA

 
 
 
 
 
 
Media Library

Press Media

 
Product category
Sector / Application
Category of company
 
Gallery view List view
[|
|
|
]  
 
 
 
Dr. Juergen M. Geissinger

CEO

Download Send to media shopping basket Larger picture
 
Dr. Juergen M. Geissinger

CEO

Download Send to media shopping basket Larger picture
 
Dual mass flywheel with centrifugal pendulum-type absorber

Dual mass flywheel with centrifugal pendulum-type absorber

Download Linked press releases Send to media shopping basket Larger picture
 
Infographics: the centrifugal pendulum-type absorber

The centrifugal pendulum-type absorber developed by LuK functions as a speed-adaptive mass damper and enables the full performance potential of modern drive systems to be exploited without sacrificing comfort.

Download Linked press releases Send to media shopping basket Larger picture
 
Torque converter

Smaller, lighter, more efficient – today’s torque converter generation is optimized for exemplary efficiency.

Download Linked press releases Send to media shopping basket Larger picture
 
Large-size bearing test stand Astraios

The four radial and four axial hydraulic cylinders (right-hand side of the picture), which generate the real loads and moments that occur in a wind turbine. The radial cylinders simulate the weight of a rotor hub with rotor blades while the axial cylinders generate the wind loads.

Download Linked press releases Send to media shopping basket Larger picture
 
Multi-function torque converter

MFTC (multi-function torque converters) are tailored to modern, charged engines and are considered as revolutionary invention in the field of torque converters.

Download Linked press releases Send to media shopping basket Larger picture
 
Large-size bearing test stand Astraios

Shortening development times and making the design process of wind turbines more reliable: The world’s largest, most up-to-date and most powerful large-size bearing test stand enables large-size bearings of up to 15 tons and measuring up to 3.5 meters such as those used in wind power applications in particular to be tested in realistic conditions using a comprehensive simulation program.

Download Linked press releases Send to media shopping basket Larger picture
 
Large-size bearing test stand Astraios

Shortening development times and making the design process of wind turbines more reliable: The world’s largest, most up-to-date and most powerful large-size bearing test stand enables large-size bearings of up to 15 tons and measuring up to 3.5 meters such as those used in wind power applications in particular to be tested in realistic conditions using a comprehensive simulation program.

Download Linked press releases Send to media shopping basket Larger picture
 
Large-size bearing test stand Astraios

Shortening development times and making the design process of wind turbines more reliable: The world’s largest, most up-to-date and most powerful large-size bearing test stand enables large-size bearings of up to 15 tons and measuring up to 3.5 meters such as those used in wind power applications in particular to be tested in realistic conditions using a comprehensive simulation program.

Download Linked press releases Send to media shopping basket Larger picture
 
Torque converter

Smaller, lighter, more efficient – today’s torque converter generation is optimized for exemplary efficiency.

Download Linked press releases Send to media shopping basket Larger picture
 
Schaeffler Pursues Holistic Approach with Regard to Electric Mobility

The eDifferential supports the steering function and has a positive effect on driving dynamics, safety and driving comfort.

Download Send to media shopping basket Larger picture
 
Inconspicuous problem solver for increasing efficiency

The overrunning alternator pulley

Download Send to media shopping basket Larger picture
 
Lightweight Differentials Create Space

The lightweight differential

Download Send to media shopping basket Larger picture
 
Dual clutch transmissions – an interplay of innovations

LuK now manufactures more than 100,000 dry dual clutches per month.

Download Linked press releases Send to media shopping basket Larger picture
 
Schaeffler Pursues Holistic Approach with Regard to Electric Mobility

The Parallel Hybrid

Download Linked press releases Send to media shopping basket Larger picture
 
Innovative thermal management module improves CO2 footprint

The temperature of the motor, turbocharger and transmission as well as the interior can be precisely controlled with the thermal management module.

Download Linked press releases Send to media shopping basket Larger picture
 
Rolling bearings are the key to optimizing friction, efficient design and optimizing start-stop systems

The rolling bearing supports reduce friction and enable a new balancer shaft design with an optimized mass.

Download Linked press releases Send to media shopping basket Larger picture
 
Schaeffler Pursues Holistic Approach with Regard to Electric Mobility

The Serial Hybrid

Download Linked press releases Send to media shopping basket Larger picture
 
Innovative thermal management module improves CO2 footprint

Rotary slide valves controlled by sensors enable the ideal temperature window for the engine and transmission to be reached quickly.

Download Linked press releases Send to media shopping basket Larger picture
 
Innovative thermal management module improves CO2 footprint

Rotary slide valves controlled by sensors enable the ideal temperature window for the engine and transmission to be reached quickly.

Download Linked press releases Send to media shopping basket Larger picture
 
Dual clutch transmissions – an interplay of innovations

LuK offers both “dry” and “wet” dual clutch solutions.

Download Linked press releases Send to media shopping basket Larger picture
 
Innovative thermal management module improves CO2 footprint

The innovative thermal management module from Schaeffler reduces fuel consumption and CO2 emissions by up to four percent.

Download Linked press releases Send to media shopping basket Larger picture
 
Innovative thermal management module improves CO2 footprint

The temperature of the motor, turbocharger and transmission as well as the interior can be precisely controlled with the thermal management module.

Download Linked press releases Send to media shopping basket Larger picture
 
Inconspicuous problem solver for increasing efficiency

The overrunning alternator pulley is one of the “unsung heroes”. This inconspicuous component reduces vibrations and improves the energy efficiency of modern engines.

Download Linked press releases Send to media shopping basket Larger picture
 
Schaeffler Pursues Holistic Approach with Regard to Electric Mobility

In the Schaeffler Hybrid, Schaeffler presents the innovative in-hub motor eWheel Drive. It also allows the development of completely new vehicle architectures.

Download Send to media shopping basket Larger picture
 
The X-life machined needle roller bearing with the Twin Cage

The X-life machined needle roller bearing with the Twin Cage: This new combination of cage and rolling elements achieves a significantly lower frictional torque.

Download Send to media shopping basket Larger picture
 
end face and rib of roller bearings

The improved contact between the end face and rib reduces the friction and significantly increases the axial load carrying capacity of cylindrical roller bearings.

Download Send to media shopping basket Larger picture
 
Deep groove ball bearings with the new FAG Generation C

Up to 35 percent less friction – the Schaeffler Group is setting the new standard for deep groove ball bearings with the new FAG Generation C deep groove ball bearing.

Download Send to media shopping basket Larger picture
 
INA thread guidance roller FRM

Lightweight and compact: The new INA thread guidance roller FRM now has a deep drawn outer ring, which means it is manufactured without cutting. The lower mass provides a considerably improved acceleration capacity.

Download Send to media shopping basket Larger picture
 
Schaeffler Pursues Holistic Approach with Regard to Electric Mobility

In the Schaeffler Hybrid, Schaeffler presents the innovative in-hub motor eWheel Drive. It also allows the development of completely new vehicle architectures.

Download Send to media shopping basket Larger picture
 
FAG high-tech Cronitect hybrid rolling bearing

The new FAG high-tech Cronitect hybrid rolling bearing: Increased load carrying capacity, smooth running and reliability.

Download Send to media shopping basket Larger picture
 
INA compacting roller OWA

Flexible: Schaeffler can supply INA compacting roller OWA without a roller covering if required. This enables customers to customize the roller to their own requirements.

Download Send to media shopping basket Larger picture
 
The Schaeffler concept vehicles

The Schaeffler concept vehicles CO2ncept-10%, Schaeffler Hybrid and ACTIVeDRIVE show the wide-ranging spectrum of modern automotive engineering and give a perspective on the extensive Schaeffler product portfolio.

Download Send to media shopping basket Larger picture
 
Linear roller bearing RUS and flat cage guidance system M/V

Linear roller bearing RUS and flat cage guidance system M/V.

Download Linked press releases Send to media shopping basket Larger picture
 
FAG spindle bearings RS

The new FAG spindle bearings RS have large size balls, a nominal contact angle of 20 degrees and an internal construction for optimized friction.

Download Linked press releases Send to media shopping basket Larger picture
 
deep groove roller bearing with Lubtect® compound

deep groove roller bearing with Lubtect® compound for a reliable supply of lubricant even under critical operating conditions.

Download Linked press releases Send to media shopping basket Larger picture
 
Profiled rail linear guides

High-speed KUVE-B-HS profiled rail linear guides offer speeds of up to 10 meters per second without losses in load carrying capacity and rigidity.

Download Linked press releases Send to media shopping basket Larger picture
 
Schaeffler lightweight differential with the axial spline

The innovative design of the Schaeffler lightweight differential with the axial spline design gives significant advantages in terms of space, weight and power consumption.

Download Linked press releases Send to media shopping basket Larger picture
 
Schaeffler components for e-mobility

The spectrum of Schaeffler components for e-mobility also includes sensor bottom bracket bearings.

Download Linked press releases Send to media shopping basket Larger picture
 
Gallery view List view
[|
|
|
]