Schaeffler Group USA Inc. · USA
 
Products LuK 

Components for Transmissions



As an engineering partner for automotive and transmission producers, LuK has access to comprehensive expertise for the entire 'transmission' system in almost all of its variants. This manifests itself in components for automated transmissions and double-clutch gearboxes, which today offer alternatives to conventional solutions and are achieved with the particular benefits of fuel consumption and dynamism. Together these transmission variants are characterised as the XSG range. But LuK has also set benchmarks in the area of Continuously Variable Transmissions (CVT) with pulleys, flat link articulated chains and controls. On the US market in particular which is traditionally dominated by automatic transmissions, LuK is also known as a specialist in torque converters and lock-up clutches and supplies vehicle and transmission manufacturers. LuK supplies systems and components to customers around the globe, with the same first-class technology, quality and delivery standards, tailored to the special requirements of our customers.