Schaeffler North America

 
 
 
 
 
 
FAQ

System requirements

Which browsers are supported?

Our online application system supports the following browsers:

  • Internet Explorer 6 for Windows XP
  • Internet Explorer 7 for Windows XP and Windows Vista
  • Internet Explorer 8 for Windows 7, Windows XP and Windows Vista
  • Internet Explorer 9 for Windows Vista and Windows 7
  • Firefox 7 for Windows 7, Windows XP and Windows Vista
  • Safari 5.1 for MAC OS X 10.6 and later
  • Chrome 15 for Windows 7

Can I contact Schaeffler regarding technical questions?

If you have additional questions or problems that could not be answered here, please send an email to Schaefflercareers@schaeffler.com.

 

Schaeffler applies cookies to secure an optimal use. With the further use of this website you accept the application of cookies. More Information

Accept