Schaeffler North America

 
 
 
 
 
 
CONTACT
PUBLICATIONS
 

Brochure | 2014-07
Bearinx® High-Level Bearing Design

 
 

Brochure | 2014-10
CABA3D
An Insight into Rolling Bearing Dynamics

 
 
PRESS

Enhanced performance in wind turbine gearboxes with bearing and system expertise

Schaeffler at EWEA 2015 in Hall P02-3

VIDEOS

Astraios – the most modern, largest, and highest performing large size bearing test rig in the world

Increased reliability and cost-effectiveness for wind turbines

 
 
 
INTERACTIVE ANIMATION
Wind Power - Interactive Animation

Find information about Schaeffler products and services for rotor shafts, gearboxes, generators, wind tracking and blade adjustments.

"Wind Power" - interactive animation

 

Simulation, Calculation and Test

Optimum design with state-of-the-art calculation and simulation programs and realistic tests

Our specialists work in close cooperation with wind turbine developers, manufacturers, and operators. State-of-the-art calculation and simulation programs ensure that optimum designs for bearings for wind power applications are produced. The entire system is considered, from individual rolling bearings and their components and adjacent construction through to the entire power transmission system, which is displayed and optimized using multi-body simulation programs developed in-house.

With its realistic force and torque simulation, Astraios has been providing valuable results since 2011, which are used for the new development of bearing solutions and for the optimization of the simulation and calculation models.

 
  SCHAEFFLER CALCULATION CHAIN
Schaeffler calculation chain: From complete systems to the rolling contact
 

From complete systems to the rolling contact

The Schaeffler calculation chain includes CAE tools that are perfectly suited to the specific requirements of the design.

  • SIMPLA : system simulation with rolling bearing expertise
  • BEARINX : bearing design with an understanding of systems
  • CABA3D : a dynamic view inside the bearing
  • TELOS : where the focus is on contact
 
SIMPLA: system simulation

SIMPLA: system simulation
With the hybrid multi-body simulation (MBS), the dynamic behavior of the entire wind turbine is displayed.

Based on the model, individual components of the drive train and the entire turbine design can be improved as early as the development phase.

  • Hybrid multibody simulation (MBS) with a non-linear, multi-dimensional coupled bearing model
  • MBS model can be derived from existing BEARINX model
 
BEARINX: optimum bearing design

BEARINX: optimum bearing design
With the BEARINX software, all bearing types, complex shafts, and shaft systems through to complete drive units can be modeled and calculated.
Amongst others, BEARINX considers the following factors:

  • Non-linear elastic deflection behavior of the bearings
  • The deflection of shafts and axes
  • The deflection of housings and adjacent components
  • The operating clearance or the preload of the bearings
  • Roller and raceway profiling as well as raceway osculation
  • Actual contact pressure considering tilted and profiled rolling elements
  • The influence of lubricant conditions, contamination and actual contact pressure on the fatigue life.
 
 
 

CABA3D: rolling bearing simulation

  • Dynamic analysis of rolling bearings
  • Determination of force and motion patterns of the rolling elements and rings, taking all degrees of freedom into consideration
  • CABA3D facilitates the calculation of the frictional energy and the acceleration behavior of the rolling elements, e.g. when they enter the load zone.
 
 
 
Close
 
 
TELOS: rolling contact simulation

TELOS: rolling contact simulation

  • 3D rolling contact simulation program
  • Any contact under general lubrication conditions
  • Quasi-stationary as well as transient load conditions
  • Coated and uncoated bearing components
 
FEM

FEM
For even more detailed analyses, FEM calculations can determine the influence of the adjacent construction on the bearings and vice-versa.

 
 
 
  LARGE-SIZE BEARING TEST RIG ASTRAIOS
Large-size bearing test rig ASTRAIOS
 

Increased reliability and cost-effectiveness for wind turbines

One of the world’s largest, most up-to-date, and most powerful large-size bearing test rigs enables bearings of up to 15 tons and measuring up to 3.5 meters to be tested in realistic conditions using a comprehensive simulation program. ASTRAIOS will result in further improvements in the understanding of systems as a whole, influencing factors and the interrelations in the drive trains of wind turbines. This means Schaeffler is making a major contribution to shortening development times for wind turbines as well as making the design process more reliable and increasing the cost-effectiveness and safety of these turbines.

The test rig has been named “Astraios” after a Titan in Greek mythology who was father of the four wind gods.

 
 
 
Close
 
 
Close
 
 

Schaeffler applies cookies to secure an optimal use. With the further use of this website you accept the application of cookies. More Information

Accept