Schaeffler Group USA Inc. · USA

 
 
 
 
 
 
Bicycles and sports equipment

Publications

RSS
Media category
Language
Search term    Please enter one or more search terms (empty space = "AND link"). Search terms with a hyphen should be placed in quotation marks (e.g. "e-business")
If you do not know the correct spelling of a term or if you want to search for families of words, it may be helpful to use so-called wildcards (*) as placeholders for syllables or characters. Wildcards can be placed at any point (e.g. linear *, deep groove * bearings) except at the start of a word.
View
   
Delivery option

Current publications

 
 
[|
|
]
 
 
Increased Comfort and Efficiency for E-Bikes
BROCHURE | 2013-01 | FSI | 036924636-0000 | ENGLISH

„Advanced by FAG“ – Increased Comfort and Efficiency for E-Bikes

FAG’s decades of experience in the development and production of bearings for bicycles are reflected in the new bottom brackets with sensors. E-bikes and pedelecs fitted with these units have a technical advantage and gain greater acceptance in the marketplace. Through precise control and top class smooth running as a result of the “Advanced by FAG” friction optimization, riding enjoyment is increased by a considerable margin.

Publisher: Schaeffler Technologies AG & Co. KG

 
State-of-the-Art Smoothness for Bicycles
BROCHURE | 2013-01 | FFL | 036842214-0000 | ENGLISH

“Advanced by FAG” – State-of-the-Art Smoothness for Bicycles

Ever since then, we have meticulously designed all of our bearing components to work together in perfect harmony, which is why our bearings usually run more smoothly than anyone else’s. Proof positive: FAG’s newly designed “Generation C” deep groove ball bearings generate 35 % less friction than the previous generation. Service life and performance are significantly increased while energy consumption is dramatically reduced.

Publisher: Schaeffler Technologies AG & Co. KG

 
BROCHURE | 2012-12 | PBO | 017215510-0000 | ENGLISH

BEARINX®-online Shaft Calculation

With our software you can now determine actual stresses while taking shaft deflection and rolling bearing deflection behavior into account. And of course, exact calculations for the internal load distribution in the bearing are performed, including contact pressure with the actual rolling element profile.

Publisher: Schaeffler Technologies AG & Co. KG

 
BROCHURE | 2012-10 | PBB | ENGLISH

BEARINX®- online Easy Ballscrew

Online calculation for screw drive bearing supports

The Bearinx®-online Easy Ballscrew module means you can now calculate screw drive bearing supports simply and quickly with Schaeffler products. The calculation program is available exclusively online and can be used free of charge.

Publisher: Schaeffler Technologies AG & Co. KG

 
TPI 215: Bottom Bracket Bearing BBRS
TECHNICAL PRODUCT INFORMATION | 2012-04 | TPI 215 | 036901571-0000 | ENGLISH

Bottom Bracket Bearing BBRS

Sensor bottom bracket bearing for e-bikes and pedelecs

The performance capability and range of e-bikes und pedelecs are determined to a significant extent by the components used. FAG has decades of experience in the development and production of bicycle bottom bracket bearings, which can be seen once again in the sensor bottom bracket bearing BBRS.

Publisher: Schaeffler Technologies AG & Co. KG

 
INA Metal-Polymer Composite Plain Bearings Durable – low-friction – economical
BROCHURE | 2011-12 | PGL | ENGLISH

INA Metal-Polymer Composite Plain Bearings

Durable – low-friction – economical

The new INA metal-polymer composite plain bearings enable economical solutions in many industrial and automotive applications. They are particularly effective with oscillating movements and achieve a rating life several times higher than that of bearings with conventional materials. In addition, all our new plain bearings are lead-free and, therefore, environmentally friendly.

Publisher: Schaeffler Technologies AG & Co. KG

 
Current-Insulating Bearings Rolling bearings for prevention of damage due to current passage
TECHNICAL PRODUCT INFORMATION | 2011-04 | TPI 206 | 036891827-0000 | ENGLISH

Current-Insulating Bearings

Rolling bearings for prevention of damage due to current passage

Current passage can occur in the use of rolling bearings in: - wheelsets and traction motors (rail vehicles); - direct current and alternating current motors (power transmission); - generators (wind power).

Publisher: Schaeffler Technologies AG & Co. KG

 
Axial Angular Contact Roller Bearings - High load carrying capacity with very small cross sections
TECHNICAL PRODUCT INFORMATION | 2010-10 | TPI 185 | 036849979-0000 | ENGLISH

Axial Angular Contact Roller Bearings

High load carrying capacity with very small cross sections

Axial ball bearings and axial cylindrical roller bearings are suitable for supporting high axial loads. However, these bearings should not be loaded in a radial direction and, on account of their cross section, require a relatively large radial installation space in the adjacent construction. Furthermore, single direction designs only support axial loads in one direction. Yet applications frequently call for compact, load-bearing and rigid solutions, which can reliably support combined loads and moments with one bearing arrangement.

Publisher: Schaeffler Technologies AG & Co. KG

 
Bearinx®-online Linear Calculation
BROCHURE | 2010-06 | PBL | 034473009-0000 | ENGLISH

Bearinx®-online Linear Calculation

Along with developing and manufacturing top quality precision parts, great service is an important tradition at the Schaeffler Group. We offer you the support you need as early as the design phase, so you can put our products into operation with confidence, because for us, service means a partnership with the customer from the first design idea right up to supplying the product.

Publisher: Schaeffler Technologies AG & Co. KG

 
“Advanced by FAG” – Improved smooth running for skaters
BROCHURE | 2010-06 | FSL | ENGLISH

“Advanced by FAG” – Improved smooth running for skaters

The main aspects of a bearing that interest skaters are: - How fast is the bearing? - How long will it last? - How does it react to environmental influences? - How heavy is it?

Publisher: Schaeffler Technologies AG & Co. KG

 
 
[|
|
]