Schaeffler North America

 
 
 
 
 
 
High-speed trains

Acela Express high-speed trains

 
 

ACELA Express is the name given to the new high-speed trains in America developed by a consortium between Bombardier Transportation (Canada) and Alstom (France). They close the gap still present in the US in the high-speed train sector in comparison to Europe (TGV, ICE) and Japan (Shinkansen). The trains operated by AMTRAK have been running since the end of 1999 on the Northeast Corridor, which is the connection between Boston and New York and reach speeds of up to 240 km an hour.

The route was overhauled and modernized so that the trains could operate at high speeds. 15 electric locomotives were purchased for traditional electrified lines alongside 18 electric motive power units (traction unit trailer with tilting traction unit).

FAG supplies all the bearings for the wheelsets, traction motors and transmissions in the traction units.

 

Schaeffler applies cookies to secure an optimal use. With the further use of this website you accept the application of cookies. More Information

Accept