Schaeffler Group USA Inc. · USA

 
 
 
 
Machine tools

Publications

RSS
Media category
Language
Search term    Please enter one or more search terms (empty space = "AND link"). Search terms with a hyphen should be placed in quotation marks (e.g. "e-business")
If you do not know the correct spelling of a term or if you want to search for families of words, it may be helpful to use so-called wildcards (*) as placeholders for syllables or characters. Wildcards can be placed at any point (e.g. linear *, deep groove * bearings) except at the start of a word.
View
   
Delivery option

Current publications

 
 
[|
|
|
|
|
|
|
|
|
]
 
 
BROCHURE | 2008-06 | PKW | 005172047-0000 | ENGLISH

Bearing Solutions for Machine Tools

With their trend-setting bearing solutions for ball screw supports, main spindles, rotary tables and linear guidance systems, INA and FAG have been leaders on the global market for decades. However, in most cases, the bearing components alone are not the decisive factors for these machine subsystems.

Publisher: Schaeffler Group Industrial

 
High precision bearings for combined loads Axial/radial bearings Axial angular contact ball bearings Axial/radial bearings with integral angular measu
TECHNICAL PRODUCT INFORMATION | 2011-11 | TPI 120 | 029097487-0000 | ENGLISH

High precision bearings for combined loads

Axial/radial bearings Axial angular contact ball bearings Axial/radial bearings with integral angular measuring system

With their forward-looking bearing arrangement solutions for feed spindles, main spindles, rotary tables and linear guidance units, INA and FAG have been at the forefront of the world market for decades. Nevertheless, bearing components alone are often no longer the decisive factor for these machine subsystems.

Publisher: Schaeffler Technologies AG & Co. KG

 
High Precision Bearings for Printing Machinery
TECHNICAL PRODUCT INFORMATION | 2011-10 | TPI 222 | 036888931-0000 | ENGLISH

High Precision Bearings for Printing Machinery

Printing machinery bearings are used in the bearing arrangements of the main cylinders in sheetfed and webfed printing machines. Due to their load carrying capacity, rigidity, accuracy and precise adjustability, they provide excellent support for the central requirement in printing machinery, namely the highest possible print quality.

Publisher: Schaeffler Technologies AG & Co. KG

 
BROCHURE | 2011-10 | PBO | 017215510-0000 | ENGLISH

BEARINX®-online Shaft Calculation

With our software you can now determine actual stresses while taking shaft deflection and rolling bearing deflection behavior into account. And of course, exact calculations for the internal load distribution in the bearing are performed, including contact pressure with the actual rolling element profile.

Publisher: Schaeffler Technologies AG & Co. KG

 
The Highest Performance Rotary Axis in the World Double the speed for rotary tables
REPRINT | 2011-09 | SSD 27 | 036926353-0000 | ENGLISH

The Highest Performance Rotary Axis in the World

Double the speed for rotary tables

For the compact bearing support of rotary tables, Schaeffler Group Industrial has improved the internal construction of the double row axial angular contact ball bearing ZKLDF to the extent that the limiting speed is double its former value. At the same time, the frictional torque is reduced while the high accuracy and rigidity of the bearing are maintained without compromise. Especially when used in combination with the new torque motors RKI from IDAM, which now also have significantly higher speeds, new possibilities are opened up in the field of turning and milling that could not previously be achieved using standard components.

Publisher: Schaeffler Technologies AG & Co. KG

 
Hybrid Axial Angular Contact Ball Bearings for Screw Drives Reliable and cost-effective
REPRINT | 2011-09 | SSD 26 | 036926388-0000 | ENGLISH

Hybrid Axial Angular Contact Ball Bearings for Screw Drives

Reliable and cost-effective

With the new hybrid axial angular contact ball bearings ZKLF..-HC, Schaeffler Group Industrial is offering a reliable solution to the problem known as “false brinelling” that has been experienced in feed spindles with ball screw drives. This means that premature bearing failures due to fluting can be avoided.

Publisher: Schaeffler Technologies AG & Co. KG

 
High Performance Rotary Axis Bearings for Combined Milling and Turning Higher rigidity and reduced friction
REPRINT | 2011-09 | SSD 24 | 036923826-0000 | ENGLISH

High Performance Rotary Axis Bearings for Combined Milling and Turning

Higher rigidity and reduced friction

The Schaeffler Group is introducing YRTC and ZKXDF, two new series of rotary axis bearings that contribute to a sustainable reduction in operating and component costs.

Publisher: Schaeffler Technologies AG & Co. KG

 
added competence 2011 / 2012
MAGAZINE | 2011-09 | ENGLISH

added competence 2011 / 2012

Performance scaled up

Performance scaled up: The best performing rotary axes in the world, Assistance on demand ensures riding pleasure: Highly efficient FAG torque sensor bottom bracket bearings for e-bikes, EMO highlights for direct drive technology: IDAM’s RKI motors make significant contribution to world’s best performing rotary axis, EMO highlights: Machine tool bearings: Rotary table bearing ZKLDF..-B – The speed doubler, EMO highlights for main spindle bearing supports: New design options for motor spindles, EMO highlights in linear technology: INA Linear Technology: Components and systems for heavy-duty linear guides, Bearing solutions for large-size machinery: Supports for rotary tables in vertical turret lathes, Safety through vigilance: FAG SmartCheck, You can count on it!: Schaeffler Group demonstrates concentrated calculation expertise with extended tools: Easy Solution, The Basics of Failure Analysis, Part 1: Fatigue, Efficiency in motion: added competence for textile machinery: The Schaeffler Group at ITMA in Barcelona, The most popular rolling elements in the world: adidas and Schaeffler Group at Technical Meeting in Herzogenaurach, Tried and tested in renewable energy applications: Bearing solutions for solar, wind and water power plants

Publisher: Schaeffler Technologies AG & Co. KG

 
PUBLICATION | 2011-09 | WL 80 375 | WL 80375 GB-D | ENGLISH

FAG SmartCheck - Safety Through Vigilance!

The Time Is Ripe: Vibration Sensors For Every Machine

FAG SmartCheck is the innovative device for ensuring the availability of all machines – today and tomorrow!

Publisher: Schaeffler Technologies AG & Co. KG

 
REPRINT | 2011-09 | SSD 06 | 034955054-0000 | ENGLISH

FAG high precision cylindrical roller bearings

FAG high precision cylindrical roller bearings are used where very high accuracy is required. Typical areas of application for these bearings include machine tools and printing machinery. They are ideal as non-locating bearings since they allow unconstrained compensation of changes in length during rotational movement between the rollers and raceways.

Publisher: Schaeffler Technologies AG & Co. KG

 
 
[|
|
|
|
|
|
|
|
|
]